No Load Detection
No Load Detection detects when a wire is disconnected from the output or a missing load
for each output point. No Load Detection occurs only when the output point is in the Off
state.
The No Load Detection feature is disabled by default. You must enable the feature in your
Studio 5000 Logix Designer application project.
Use the diagnostic assembly to monitor the presence of a No Load condition.
Provide Feedback