Data Readback
Data Readback automatically sends point data values that read back the output at the
screw, regardless if it matches the digital value that was sent to the screw terminals
of the module then.
The read back value is either On or Off.
Fault and status data are also sent. This data is sent at input RPI.
Provide Feedback