Reset to Out-of-Box Configuration
When the Studio 5000 Logix Designer application is online, the Safety tab of the Module
Properties dialog box displays the current configuration ownership. When the opened
project owns the configuration, Local is displayed.
When a second device owns the configuration, Remote is displayed, along with the SNN, and
node address or slot number of the configuration owner. Communication error is displayed
if the module read fails.
If the connection is Local, you must inhibit the module connection before you reset
ownership.
Provide Feedback