Standard Module Applications
This chapter describes how to configure your standard digital I/O modules in a Studio
5000 Logix Designer application project. You can use the default module configuration or
edit the module configuration.
This chapter does not explain the user-configurable module features that you can edit on
different screens in your Studio 5000 Logix Designer application project.
Provide Feedback