Contactor/Starter Information - Predictive Maintenance View
The Predictive Maintenance view displays predictive maintenance data for the device. Predictive maintenance data is blank when offline.
Starter Predictive Maintenance

Parameter | Option |
|---|---|
View as | This is a display filter that displays predictive maintenance data according to the selected option:
|
Status | Values are:
|
Elapsed life/Remaining life/Consumed life | Depends on View as dropdown selection: Shows the elapsed life, remaining life, or Consumed life percentage in terms of operations for switching device and hours for PCB assembly. |
Location | Identifies the location of the component within a product, device, or subsystem. |
Catalog number | Shows the device catalog number. |
Reset | Resets the predictive maintenance data. |
Settings | Displays the predictive maintenance settings dialog box. |
Refresh | Manually refreshes the predictive maintenance data when online with the device. |
Predictive Maintenance Settings
Predictive Maintenance Settings displays options to set indicators and messages and configures the alarm for the remaining life threshold percentage.
Predictive Maintenance Settings

Parameter | Description |
|---|---|
Predicted life | Displays the Maximum life and the Remaining life threshold. |
Alarm notification | Enables the remaining life below threshold alarm. If not selected, the alarm is not set even if the alarm threshold is crossed. |
Remaining life threshold | Sets the remaining life threshold as the percentage of Maximum life. Values
allowed:
Remaining life varies according to selected threshold values. |
Provide Feedback