Contactor/Starter Information - Online Values View

The Online Values view displays the states for the device. The information depends on the starter type.
Online Values Status Indicators
Status Indicator
Description
Indicates the status is active for data read from the device. For example, the starter is active in forward direction, or the interlock is active.
Indicates the status is inactive for data read from the device. For example, the starter is not active in forward direction.
Indicates an error condition. For example, the interlock signal is inactive.
Data read from the device indicates a warning condition exists.
Starter Online Values (100-E-INT-D shown)
Starter Online Values
Device Type
Starter
Local Input
HOA Status
100-E-INT-D Non-Reversing Starter Interface
On
Interlock
When Controlled by is set to Controller/Peer 2-Wire or Controller/Peer 3-Wire:
  • Hand
  • Off
  • Auto
104-E-INT-D Reversing Starter Interface
  • Forward
  • Reverse

Online Values View - 100/104-E-INT-X Modules

The 100-E-INT-X and 104-E-INT-X communication modules have additional online value information.
Starter Online Values (100-E-INT-X shown)
Device Type
Starter
Warnings
Trips
Local Input
HOA Status
100-E-INT-X Non-Reversing Starter Interface
  • Forward
  • Motor current
If StarterType value = 9...15:
  • Circuit Breaker
  • Phase loss
  • Underload
  • Overload
  • Jam
  • Phase loss
  • Underload
  • Overload
  • Jam
  • Test
If StarterType value = 9...15:
  • Short Circuit
  • Contactor Weld
  • 140M-E
Interlock
When Controlled by is set to Controller/Peer 2-Wire or Controller/Peer 3-Wire:
  • Hand
  • Off
  • Auto
104-E-INT-X Reversing Starter Interface
  • Forward
  • Motor current
  • Reverse
If StarterType value = 9...15:
  • Circuit Breaker
Utilization (100-E-INT-X shown)
Utilization is a view only available to 100/104-E-INT-X modules. It provides additional monitoring information.
Utilization (100-E-INT-X shown)
Device Type
Current
Overload
Application
100-E-INT-X Non-Reversing Starter Interface
  • Average current
  • L1 current
  • L2 current
  • L3 current
  • TCU
  • Average FLA
  • Trip class
  • FLA
  • Auto reset
104-E-INT-X Reversing Starter Interface
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal