Contactor/Starter Information - Device Information View

Use the Device Information view to view device and status information when the device is online. Use the Device Information view to do the following:
  • Determine the identity of the device.
  • View the device's current operational state.
  • View whether the device was configured by the owner controller.
  • View whether an owner controller is connected to the device.
  • Retrieve the status from the device.
  • Reset a device to its power-up state.
  • If supported, view the Protection Mode of the device.
Starter Device Information
Starter Device Information
The data in the Device Information view comes directly from the device.

Device Locator Dialog

Use this dialog to define a user-defined period of time to identify a device:
  • Duration: Select the Minute and Seconds durations from the dropdown lists.
  • Blink: Click Blink to update the system status indicator for the selected time period.
Starter Device Locator
Starter Device Locator
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal