Module Properties - General for ETHERNET-PANELVIEW
Use this tab to create/view module properties for the ETHERNET-PANELVIEW EtherNet/IP
PanelView
.On this tab, you can:
- view the type and description of the module being created
- view the vendor of the module being created
- view the name of the parent module
- enter the name of the module
- enter a description for the module
- enter the minor revision for the module
- select Exact Match, Compatible Module, or Disable Keying
- enter the IP address and host name for the module
- view the status the controller has about the module (you can only view the status while online)
Parameters
Type
Displays the type and description of the module being created (read only).
Vendor
Displays the vendor of the module being created (read only).
Parent
Displays the name of the parent module.
Name
Enter the name of the module.
The name must be IEC 1131-3 compliant. This is a required field and must be completed; otherwise you receive an error message when you exit this tab. An error message is also displayed if a duplicate name is detected, or you enter an invalid character. If you exceed the maximum name length allowed by the software, the extra character(s) are ignored.
IEC-61131 Name Standard
(The names are composed per IEC-61131, section 2.1.2.)
An identifier is a string of letters, digits, and underline characters that begin with a letter or underline character. Underlines are significant in identifiers (for example, A_BCD is interpreted differently than AB_CD). Multiple leading or multiple (consecutive) embedded underlines are not allowed, trailing underlines are not allowed, and letter case is not considered significant.
TIP:
In Logix Designer, most component names are limited in length to 40
characters or less.
Description
Enter a description for the module here, up to 128 characters. You can use any printable character in this field. If you exceed the maximum length, the software ignores any extra character(s).
Comm Format
Select the communication format for the module. This field lists the available formats.
Revision
Select the minor revision number of your module.
The revision is divided into the major revision and minor revision. The major revision is used to indicate the revision of the interface to the module. Valid values are in the range from 0 to 127. The minor revision is used to indicate the firmware revision. Valid values are in the range from 0 to 255, with 1 being the default value.
Electronic Keying
Electronic Keying
Electronic Keying reduces the possibility of using the wrong device in a control system. Electronic Keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
These attributes are compared:
Attribute | Description |
Vendor | The device manufacturer. |
Device Type | The general type of the device, for example, digital I/O module. |
Product Code | The specific type of device. The Product Code maps to a catalog number. |
Major Revision | A number that represents the functional capabilities of a device. |
Minor Revision | A number that represents behavior changes in the device. |
For more information on Electronic Keying, see Electronic Keying in http://literature.rockwellautomation.com/idc/groups/literature/documents/at/logix-at001_-en-p.pdf Control Systems Application Technique, publication LOGIX-AT001.
IP Address
Enter the IP address of the module.
IP address
- The Internet Protocol (IP) address identifies each node on the IP network (or system of connected networks). Each TCP/IP node on a network (including the Ethernet module) must have a unique IP address.
- The IP address is 32 bits long and consists of a net ID part and a host ID part. Each network is a Class A, Class B, or Class C network. The class of a network determines how an IP address is formatted.
- Each node on the same physical network must have an IP address of the same class and must have the same net ID. Each node on the same network must have a different host ID, thereby giving it a unique IP address.
- IP addresses are written as four decimal integers separated by periods (i.e., xxx.xxx.xxx.xxx), where each integer (or xxx) is a number between 0 and 255 which gives the value of one byte of the IP address.
- The first octet of the IP Address may not be 127, or a number greater than 223.
For example, the 32-bit IP address:
00000011 00000000 00000000 00000001 is written as 3.0.0.1.
Distinguish the class of an IP address from the first integer in its dotted-decimal IP address as follows:
Range of first integer | Class of network |
0 - 127 | A |
128 - 191 | B |
192 - 223 | C |
224 - 255 | other |
TIP:
You must enter either an IP address for the module OR a host name. You do not have to enter both. These items are mutually exclusive; once you choose one, the other will be disabled.
Host Name
Enter host name for the module.
host name
The host name is the unique name that identifies a computer on a network.
On the Internet, the host name is in the form comp.xyz.net. If there is only one Internet site, the host name is the same as the domain name.
One computer can have more than one host name if it hosts more than one Internet site (for example, home.xyz.net and comp.xyz.net). In that case, home and comp are host names and xyz.net is the domain name.
Valid characters consist of:
- Numbers in the range of 0…9
- Alpha characters in the range of A…Z (upper or lower case)
- dash
- period
- No more than 64 valid ASCII characters
- The first character of the host name must be an alpha character (in the range of A…Z (upper or lower case))
- The last character of the host name cannot be a period or a dash
- The host name cannot contain two periods next to each other
Examples of legal host names include:
- HostName.com
- HostName
- HostName.123
- Host-2-Name.com
- HostName.DomainName.com
- Host123Name456.789DomanName000.com
Examples of illegal host names include:
- .HostName.com
- HostName.com.
- HostName..com
- HostName.com-
- 123.com
- 1234567890
TIP:
You must enter either an IP address for the module OR a host name. You do not have to enter both. These items are mutually exclusive; once you choose one, the other will be disabled.
TIP:
The
Host Name
parameter is not available when you configure safety
devices. Host names require DNS lookup, which is not allowed for safety devices. Input Assembly Instance
Produces multi-cast input data. Specify this assembly instance when opening a connection. Valid values are:
- AI1 (corresponds toLogix Designerinstance 7) - this is the default value
- AI2 (instance 9)
- AI3 (instance 11)
- AI4 (instance 13)
- AI5 (instance 15)
- AI6 (instance 17)
- AI7 (instance 19)
- AI8 (instance 21)TIP:This value is independent of the value you choose for Output Assembly Instance.
Input Assembly Size
Enter the number of 16-bit input words required for communication with the module. Valid values range from 1 to 225, depending on the Comm Format you have chosen.
Comm Format | Valid Values | Default |
Data - INT | 1-225 | 225 |
Input Data - INT | 1-225 | 225 |
Data - DINT | 1-112 | 112 |
Input Data - DINT | 1-112 | 112 |
Output Assembly Instance
Consumes output data. Valid values are:
- AO1 (corresponds toLogix Designerinstance 6) - this is the default value
- AO2 (instance 8)
- AO3 (instance 10)
- AO4 (instance 12)
- AO5 (instance 14)
- AO6 (instance 16)
- AO7 (instance 18)
- AO8 (instance 20)TIP:This value is independent of the value you choose for Input Assembly Instance. This field is disabled if you have chosen either the Input Data - INT or the Input Data - DINT comm format.
Output Assembly Size
Enter the number of 16-bit output words required to communicate with the module. Valid values range from 1 to 225, depending on the Comm Format you have chosen.
Comm Format | Valid Values | Default |
Data - INT | 1-225 | 225 |
Data - DINT | 1-112 | 112 |
Provide Feedback