Cubic button

Select this button to change the selected cam segment to cubic type. The cam segment is the path from one cam point to the next cam point. When all cam segments are cubic, this button is disabled.
TIP: Selecting a also selects the cam segment which follows it, so that both the cam point and cam segment are highlighted. The cam point is a position within a cam profile determined by the coordinates of the master and slave.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal