Friction page
Use the settings on the
Friction
page to:- Enter the percentage of sliding friction for the load of the motor.
- Enter the friction compensation window position.
TIP:
To open the Friction page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, expand theLoadfolder, and then selectFriction.
These are the
Friction
page parameters.Parameter | Description |
|---|---|
Sliding Friction Compensation | Specifies the percentage of sliding friction for the load in % Rated units. |
Compensation Window | Specifies the compensation window position in terms of user define position units. |
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.
TIP:
The
Parameter List page may contain
more attributes than the associated page. In some cases, attributes that display
on the Parameter List page do not display on the associated page. |
Provide Feedback