Show All Actions in Routine command
Choose this command to display all actions associated with all steps within a routine. If you choose this command, you can click the - sign to temporarily hide the action when you don’t need to view it.
Note that if you choose this command, the setting applies to all steps in the routine, is stored in both the online and offline projects, and is saved for future editing sessions. To undo this command, choose the Hide All Actions in Routine command.
Provide Feedback