About outlining in Structured Text routines

Use outlining to organize a Structured Text routine into collapsible segments. Define segments automatically using automatic outlining, or by marking specific regions.
When automatic outlining is enabled, the editor creates a collapsible outline segment when a line starts with
#region
,
if
,
while
,
repeat
,
for
, and
case
, and ends with the matching end construct, such as
#endregion
or
end_if
.
View the contents of a collapsed segment without expanding it by hovering the cursor over the segment. To expand and collapse all the segments in a routine at once, on the main menu, select
Edit > Outlining > Expand all outlining
or
Edit > Outlining > Collapse all outlining
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal