PLLS motors in service
Use the
Motors in service
tab on the PLLS Properties
dialog box to select the motors that are in service for Process Lead Lag Standby Motor Group (PLLS) instructions.To select the motors in service for PLLS instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- UnderAdvanced, select theMotors in servicetab.
- Select the check box beside a motor to put it in service. Clear the check box to remove the motor from service.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state:
- None
- Stopped
- Running
- Stopping
- Decreasing
- Increasing
- Device issues. Displays fault conditions:
- None
- Configuration error
- Fail to start
- Fail to stop
- SelectApply.
Provide Feedback