HMI text for PLLS instructions
Use the
HMI
tab on the PLLS Properties
dialog box to enter text that appears on HMI devices for Process Lead Lag Standby Motor Group (PLLS) instructions. To enter HMI text for PLLS instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theHMItab.
- Configure these settings:
- Library name. Associates instructions with a display library for faceplate call-up.
- Instruction name. Associates the instruction name for faceplate call-up.
- Display label. A label that appears on the graphic HMI symbol.
- Area name for security. The area name for area-based security in the HMI.
- Help button URL. URL for accessing help from the HMI.
- Enable navigation to permissive object. Enables navigation from the HMI to a permissive object faceplate.
- Enable navigation to interlock object. Enables navigation from the HMI to an interlock object faceplate.
- Enable navigation to an object with more information. Select this checkbox to enable navigation to another source of information. In the box, enter the navigation path to the object, document, or website.
- Operator command confirmation required. Configure operator commands and settings to require confirmation or to apply an e-signature from the HMI. Select:
- None–command requests do not require confirmation by the operator.
- Command confirmation–command requests require confirmation by the operator. This option displays a dialog asking the user to confirm the action.
- Performer e-signature–command requests require an operator signature. This option enforces security from the HMI and disables commands and settings from the Logix Designer dialog.
- Performer and approver e-signatures–command requests require both operator and supervisor signatures. This option enforces security from the HMI and disables commands and settings from the Logix Designer dialog.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state:
- None
- Stopped
- Running
- Stopping
- Decreasing
- Increasing
- Device issues. Displays fault conditions:
- None
- Configuration error
- Fail to start
- Fail to stop
- SelectApply.
Provide Feedback