Change the firmware revision

To change the firmware revision for which the current project is configured:
  • On the
    Change Revision
    dialog box, enter the number of the major firmware revision for which you want this project to be configured.
    The list of available revisions includes all software major revisions that are installed, and that are greater than the current revision.
  • Select
    OK.
    You are prompted to save your changes; note that doing so also saves any other changes you have made in the controller properties.
A backup of the project file is made with the old version in the name (for example, test_project.acd_v10).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal