Print Options dialog box - Equipment Sequence Listing
You use the
Print Options dialog box - Equipment Sequence Listing
to adjust the print layout settings for an Equipment Sequence report.
TIP:
To open the Print Options dialog box - Equipment Sequence Listing:
- SelectFile > Print Options.
- When the Print Options dialog box opens, selectEquipment Sequence Listingin the Categories pane.
The dialog box contains the following settings.
- Shrink to Fit Page- Select this check box to set the magnification so that the report fits on one page.
- Include Blank Sheets- Select this check box to include all pages in the report, including blank sheets. Blank sheets sometimes appear when they are needed to make a complete rectangular field for the sequence diagram. In the following example, a blank sheet is included to complete the sequence diagram.

Provide Feedback