Equipment Phase Properties - Parameters Tab fields
Use the dialog to create or modify the execution of the equipment sequence. These options are available in the
Parameters
tab of the Equipment Phase
PropertiesParameters
tab.
Name | Purpose | |
![]() | Name | View or edit the name of the parameter. |
![]() | Usage | Select a Local tag or an Input, Output, InOut, or Public parameter. Use this column to switch to another valid usage type.
|
![]() | Sequencing | Select this option to designate the tag as a sequencing parameter. Only Input and Output parameters can be used by an Equipment Sequence . Sequence Manager and FactoryTalk Batch communicate with the Equipment Phase through parameters with the Sequencing attribute selected. |
![]() | Data Type | Choose from the list of data types. The ALARM_ANALOG, ALARM_DIGITAL, AXIS_CIP_DRIVE, AXIS_CONSUMED, AXIS_GENERIC, AXIS_GENERIC_DRIVE, AXIS_SERVO, AXIS_SERVO_DRIVE, AXIS_VIRTUAL, COORDINATE_SYSTEM, MESSAGE, MODULE, and MOTION_GROUP data types do not support arrays. Only use these data types in controller scope, except for:
If the tag has a Usage of Input or Output and Sequencing is selected, the tag must have one of these Data Type :
|
![]() | Connections | Choose the browse button to navigate to the Select Tag dialog and select the tag to make a connection. |
OK | Select to accept edits. If all attributes are valid, the modified attributes save for the current Equipment Phase and the dialog closes. OK and Apply are not available if the dialog contains invalid data. | |
Cancel | Select to cancel edits and close the Equipment Phase Properties | |
Apply | Select to apply edits and continue editing in the Equipment Phase PropertiesOK . |
Provide Feedback