Reference Add-On Instruction Information by Logic
Use the
By Logic
tab on the Cross Reference
dialog box to navigate to specific logic in an Add-On Instruction.To reference Add-On Instruction Information by Logic:
- PressCtrl + Eto open theCross Referencedialog box.
- On theTypemenu, selectAdd-On Instruction.
- On theNamemenu, select an Add-On Instruction.Each individual call to the selected instruction is listed, sorted in ascending order by container name. Double-click an element of the list to navigate to the location.
- Double-click a column header to sort information.References inside source-protected and license-protected Add-On-Instructions indicate that the Add-On-Instruction may be affected by changes to the definition of the selected Add-On-Instruction. However, theRoutine,Location, andTagcolumns are blank andSource Not Availableappears in theDescriptioncolumn. Attempting to navigate to logic in a source- or license-protected Add-On Instruction opens the definition editor for the Add-On Instruction.Information in each column:ColumnDescriptionContainerThe program, phase, or instruction in which the Add-On-Instruction is referenced. Icons indicate container types.RoutineThe routine containing the reference.LocationThe location of the reference within the routine. When an Add-On Instruction is locked, this column displaysSource not available.TagThe name of the tag referenced by the call to the instruction referenced by the invocation.DescriptionThe description of the backing tag, including pass-through if one is configured.
Provide Feedback