Geolocation
    The Geolocation allows you to locate any remote devices registered to a domain.
The public IP addresses of the devices allow for their geolocation. Each device shown in the map is represented by a 
pushpin
. Multiple devices sharing the same public IP address are grouped together and represented through a single pushpin
 .
     NOTE: 
    See Explorer for further information on this subject.
Provide Feedback