Audit
    The 
Audit
 section allows you to view any connections to remote devices and the users who established them, as well as any management operations carried out by users on domain entities.Operations
       section allows you to view all the operations carried out within the domain.
You can access the  operations log by accessing . This log reports a variety of device-related operations, such
        as registration, renaming, moving to other folders, permissions assignments, etc.
FactoryTalk®
            Remote Access™
 ManagerThrough the filter bar at the top, it is possible to select the log reference period and filter out search results. The table located below the filter bar returns the desired results, including a small operation description.
You can download the log into a .csv or .xls spreadsheet, by clicking the  button at the top right of the screen.
 button at the top right of the screen.
See a brief filters overview in the following table:
| Filter | Description | 
| Author name | The user that performed the operation. | 
| Operation type | The list of available operations in a specific domain. | 
| Target type | The component type affected by a specific operation. | 
| Target name | The username of the user account that performed the listed operations. | 
| Result | It groups operations by their outcome. | 
| Date from | It sets a filter start date. | 
| Date to | It sets a filter end date. | 
Connections
      You can access information on the remote device connections by selecting .
A table returns the desired results, including details about the connection duration. Double-click each connection row. A screen appears listing all the operations carried out by the selected user. You can then filter the results for a refined search and possibly export it.
By clicking 
Operation type
, connection details can be filtered by means of a context menu, including further details, such as chat messages, connection start and end, etc.You can download the log into a .csv or .xls spreadsheet by clicking the  button at the top right of the screen.
 button at the top right of the screen.
See a brief filters overview in the following table:
| Filter | Description | 
| User account name | The user that started the connection. | 
| Device | The device for which connection information is to be retrieved. | 
| Date from | It sets a filter start date. | 
| Date to | It sets a filter end date. | 
     NOTE: 
    
The time information is provided in local time and time zone, where:
- The Local time refers to the time when the query was raised by the local device.
- The Time zone refers to the UTC offset.
     TIP: 
    Click the 
Details
 button to view information about each single device connection.Provide Feedback