(Interactive Access) Log
    This section lists all of the operations that are being carried out through the 
Interactive Access
 Tool. It allows you to view and export any connection logs and the list of activities executed during remote assistance sessions. It is possible to establish more connections simultaneously from the same Interactive Access
 Tool, as each device is instantiated.In fact, the 
    
Log
 section shows that the operations carried out by all
      of the connected devices. Nevertheless, Interactive Access
 generates as
      many logs as the quantity of connected devices and stores them in a folder that you can access
      by clicking the Open log folder
 button. 
     NOTE: 
    The same folder also
        includes the operation logs generated by other  Tools, however these latter do not feature
        a button directly linked to this folder. See FactoryTalk Remote Access Manager Tools
        for further information on this topic.
FactoryTalk®
            Remote Access™
In Linux devices, you can export the connections logs in .txt format by clicking on the 
Export device logs
 button. These logs contain the information displayed in the Log
 section.Each log file name is made up of a unique device identifier and a final digit (that may feature decimals), from 1 to 3.
      
    
     NOTE: 
    The final digit following the unique device identifier stands for the log file version. In fact, every log file greater than 1MB is overwritten, and its version digit is progressively updated.
Considering that it is not always possible to record any operations associated with a device, a generic 
DeviceConnectionApplet
 log records any applet operations whenever no device is connected.The log folder can store log files up to 10 MB.
Provide Feedback