Remote Access Tools Security
    
    FactoryTalk®
          Remote Access™
VPN
      Once a Tools Applet client is connected to a Runtime client, a VPN connection can be established depending on how the “VPN access” permission is given to a user on a given device.
The  VPN
        works at level 2 of the ISO/OSI protocol stack, that is, it encapsulates Ethernet frames
        instead of IP packets. This is done for best compatibility with common industrial scenarios,
        where non-IP protocols or broadcast messages are used.
FactoryTalk®
            Remote Access™
The VPN is implemented by installing a virtual Ethernet adapter on the Frontend PC.
FactoryTalk®
            Remote Access™
FactoryTalk®
            Remote Access™
Even if level 2 is below IP, by default the Runtime service automatically assigns a free IP to the Frontend virtual VPN adapter. This is done for convenience, since most useful protocols are IP based and thus ready to work. Moreover, IPs from the actual physical subnets are used. No virtual IP subnets and consequent routing rules are created.
The Runtime periodically polls for existing devices on the network by sending ARP messages. It discovers “free” IPs that can be later assigned to VPN connections. This policy is handy but can be changed if a stricter and more controlled configuration is needed. An IP pool can be configured on the device so the Runtime will only assign IPs coming from this pool. In this case, no ARP discovery is performed.
Having the Frontend PC virtually connected to the physical device network is powerful and useful, but it can be configured and limited in several ways to comply with ICT policies.
VPN firewall rules can be configured in the  to control what kind of traffic of a certain combination of
        device/sub-device/user/protocol can be remotely used. These rules can be obtained by
        configuring firewall rules across the organization hierarchy. Rules are hierarchical,
        per-user, per-resource, or per-resource group, and can be limited to a certain remote MAC
        address, remote IPs, subnets, and Ethernet or IP protocols, in an ALLOW – DENY fashion. The
        resulting set of rules is calculated by the server before a VPN connection starts and are
        enforced on both Frontend and Runtime.
FactoryTalk®
            Remote Access™
 organizationThe best practice regarding security is to enable only the protocols and reachable
        destination needed by a specific remote user or user group. This makes the VPN connection
        even more secure than an actual physical local connection, because in a physical connection,
        the local PC firewall is the only mechanism to limit traffic. In our case, the 
        infrastructure takes care of enforcing the security rules decided by the administrator.
FactoryTalk®
            Remote Access™
File Transfer
      Remote file operations (download, upload, rename, delete) are served through the  Service
        process. This process is running with local system privileges by default. In any case, the
          
        organization admin can enable or disable this operation for remote users depending on how
        the File Transfer permission is propagated to a particular device for a specific user.
FactoryTalk®
            Remote Access™
FactoryTalk®
            Remote Access™
Device registration to Domain / Configuration Via Local Network
      The registration to a domain or the configuration can be carried out using specific applets that work on the local network. These applets use an AES-256 GCM algorithm to encrypt the network traffic.
Provide Feedback