Launch a service
    You can launch a subdevice service through a specific
        .
Services
 section in the FactoryTalk®
          Remote Access™
 Manager- In , select the subdevice.
- On the right pane, expand theServicessection to view all of the subdevice services.
- Select the service that you want to initiate and clickLaunch.TheInteractive AccessTool automatically establishes a VPN connection with the device to which the subdevice is connected. In this way, you are granted access to the device subnet, so you can reach the subdevice and make its service run.
Provide Feedback