Create a domain subfolder
    domain subfolder
Domain subfolders
 can be
      managed by selected administrators and can be accessed by a restricted group of users. This is
      useful if you are collaborating with different vendors or if you are managing a variety of
      operations through FactoryTalk®
          Remote Access™
 Manager
     NOTE: 
    See Organizations, domains and domain subfolders and FactoryTalk Remote Access Manager overview and related entities for further information on this subject.
To create a 
domain subfolder
 proceed as follows:- Log on towith an administrator user account.FactoryTalk® Remote Access™Manager
- Access the section.
- Select theAdd resource(circled plus) button andCreate folder.
- Add any user accounts for the administration of the newly created folder.
- Ensure that the admin user accounts haveAdminpermissions to the folder.
When a local contributor signs in to 
FactoryTalk®
        Remote Access™
 Manager, they will only be able to work with
      the domain subfolder that they have been granted permission to. They will not be able to see
      any other folders that were created by the domain administrator. However, within the folder
      they administer they will be able to add any groups, devices, and additional domain
      subfolders as necessary.Provide Feedback