Basic entitlement on ASEM 6300 iPC
    entitlement
 on ASEM 6300 iPC
The Access Server assigns a Basic entitlement to Windows FTRA Runtimes on these devices.
To upgrade a Basic entitlement for any 
FactoryTalk®
        Remote Access™
 Runtime installed on any ASEM hardware:- Access FactorytalkHub.com and clickUpgradenext to the Basic entitlement that you own.
- Choose a Pro entitlement from the available entitlements list.
     NOTE: 
    The Pro entitlement deactivation restores the Runtime Basic entitlement.
     NOTE: 
    Basic entitlements are set as per factory settings.
Provide Feedback