Connect FactoryTalk Design Studio to FactoryTalk Remote Access
    FactoryTalk Design Studio uses a custom FactoryTalk Remote Access user named 
      
    
FTDS
 to communicate to on-premises devices through FactoryTalk Remote Access endpoints. To confirm this user’s configuration, see Enable FactoryTalk Remote Access for FactoryTalk Design Studio. Access to the Build and Deploy Center requires the Engineer role. To modify communication configuration, a FactoryTalk Design Studio Core entitlement is required.
      To connect FactoryTalk Design Studio to FactoryTalk Remote access, once the FactoryTalk Remote Access configuration is complete:
- With a controller added to your project, (see Add a controller), go to theDeployment Centerto set the path to the controller.
- Select the hamburger menu in the path field. The Set Device Pathscreen appears.The list of drivers on this screen is common to all users and all FactoryTalk Design Studio projects in your FactoryTalk Hub organization. in the path field. The Set Device Pathscreen appears.The list of drivers on this screen is common to all users and all FactoryTalk Design Studio projects in your FactoryTalk Hub organization.
- Select the plug icon to configure a new driver. The Configure Driversscreen appears. to configure a new driver. The Configure Driversscreen appears.
- TheAvailable Driver Typesshown should beFactoryTalk Remote Access (VPN). SelectAdd New. TheChange the VPN Endpointscreen appears and shows the FactoryTalk Remote Access endpoints that haveFTDSuser permissions assigned to them.
- Select the FactoryTalk Remote Access endpoint or device to which you want to connect. The on-premises controller must have a network connection to this endpoint to be visible to FactoryTalk Design Studio.
- The default discovery method for a new VPN connection isDevice List/Range. To use this method, you must add a specific IP address or range of IP addresses in theDevice List/Rangefield of this dialog box. If these addresses are not known or you prefer an automatic discovery, change the Discovery Method toBroadcast. Broadcast discovery finds all available controllers connected to the selected endpoint.
- ClickOKto add your new endpoint. You are returned to theConfigure Driversscreen.
- SelectClose.Your new endpoint now appears in theSet device pathlist and is available to all projects within your organization.
- Right-click on the endpoint and selectConnectfrom the menu which appears. This establishes an active connection to the FactoryTalk Remote Access VPN endpoint, and a list of all available controllers connected to that endpoint appears.
- Once connected, expand the list to see available controllers.
- Highlight the controller whose path you want to set and selectOKto set the path. You can now connect to and deploy to your controller from FactoryTalk Design Studio.
 FactoryTalk Design Studio is now configured to communicate through your FactoryTalk Remote Access endpoint, and you’ve set your on-premises controller path. 
Provide Feedback