Station Runtime (XS)
This XS example shows you a system architecture using an Embedded Edge Compute module.
XS System architecture
This example architecture has the following components:
- No HMI displays
- Communicates with aRockwell Automation®controller
- Acts as an OPC UA server
- Logs data to an internal database
- One web client
The following picture shows example runtime sizing for a package that includes these application components.
XS with Embedded Edge Compute module

Provide Feedback