Deployment Guidelines

After you create your project, you must deploy it to a target device. This section helps you deploy it correctly.
  1. Confirm that the
    FactoryTalk® Optix
    Application Update Service runs on the target device.
    The Application Update Service is part of the
    FactoryTalk® Optix
    Runtime Tools.
    OptixPanel
    and Embedded Edge Compute devices come with Runtime Tools preinstalled. You must install the Runtime Tools on other target devices.
  2. To operate correctly, the Application Update Service requires the TCP port 49100 to be reachable and a valid username with a configured password.
  3. Configure a Target Device to accept the application. The Application Update Service requires that a firewall is configured in a way that TCP port 49100 is reachable. The target device username and password are needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal