FactoryTalk® Optix Studio
User Interface

FactoryTalk® Optix
Design Environment
Main screen for FactoryTalk Optix Design Environment software.
FactoryTalk® Optix
Design Environment
Interface Section
Description
A
Main toolbar
B
Project panel displays project information model to display and set the structure of nodes. The nodes can be organized according to parent/child logics
C
Types panels with details on:
  • Essential types, which are grouped in folders according to their purpose
  • Custom project types, which are located in folders that reflect the project structure
D
Log panel displays messages that are related to the operation of the software
E
Path of the object being edited in the editor
F
Toolbar specific to the object type being edited
G
Object editor to set interface objects or to configure other specific object types (such as tag importers or recipes)
H
Properties panel displays the properties of the selected node in the Project or in the object editor
I
Events panel to subscribe methods to events that can be generated
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal