Numeric data query examples

Numeric data query examples

Sample queries for filtering motors based on different properties.
Display Motor5 object
SELECT * FROM Model WHERE BrowseName = 'Motor5'
Display motors with Acceleration of 20
SELECT * FROM Model WHERE Acceleration = 20
Display motors with Acceleration of 20 and Speed between 300 and 500
SELECT * FROM Model WHERE Acceleration > 20 AND Speed BETWEEN 30 AND 500
Display motors of Names that start with
Faulty
SELECT * FROM Model WHERE BrowseName LIKE 'Faulty%'
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal