Fault Action view parameters

Parameter
Description
Output KYZ, R1, R2, R3 / Output State During Communications Fault
Specifies the action the power monitor takes on the respective output if an active Data Connection faults.
The available values are:
  • 0 = Hold Last State and Resume (default)
  • 1 = Hold Last State/Freeze
  • 2 = De-energize and Resume
  • 3 = De-energize/Freeze
  • 4 = Local Control
Tip:
Freeze = maintain state of output when communications recovers until one of the following occurs:
  • Logic controller enters program mode
  • Power cycle to the power monitor
  • Change the parameter value to
    Resume
When an internal Power Monitor failure occurs:
Instructs the power monitor how to respond to an internal failure.
Select from:
  • Power Monitor Resets and resumes operation
  • Set outputs to off, stop communications with Controller and enter Safe Mode
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal