Failed to modify device definition

Possible error messages:
  • Failed to modify device definition. Input size limit will be exceeded.
  • Failed to modify device definition. Output size limit will be exceeded.
  • Failed to modify device definition. Configuration size limit will be exceeded.
  • Failed to modify device definition. Input and output size limits will be exceeded.
  • Failed to modify device definition. Input and configuration size limits will be exceeded.
  • Failed to modify device definition. Output and configuration size limits will be exceeded.
  • Failed to modify device definition. Input, output, and configuration size limits will be exceeded.
Possible cause and solution:
  • Exceeded one or more size limits (input, output, or configuration). Size is the sum of command variable, device variables, and dynamic variables.
  • Remove command or device variable or reduce the number of dynamic variables.
The input and output size limits are 228 bytes. The configuration size limit is 350 bytes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal