Overview view parameters

The
Overview
view includes these parameters.
Parameter
Description
Expanded device type
Displays the four-digit hexadecimal device type.
Shows
Unspecified
when
Use expanded device type
checkbox is cleared in the
Device definition
checkbox.
Revision
Displays the HART device revision and HART software version.
Shows
None
when the
Use expanded device type
checkbox is cleared in the
Device definition
checkbox.
Electronic keying
Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
Valid values include:
  • Exact Match
  • Compatible Module
  • Disable Keying
For detailed information on Electronic keying, see Electronic Keying in
Logix5000
Control Systems Application Technique
, publication LOGIX-AT001.
Connection
Displays the connection type and the communication format.
Device definition
Opens
Device definition
to change the revision, electronic keying, and other device specific values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal