Device definition dialog box - Variables view

In the
Device definition
dialog box, use the
Variables
view to configure the dynamic variables of the device.
TIP:
The
Available device variables
and
Selected device variables
lists only appear when an expanded device type is specified and the associated EDD file is available.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal