Connection view

Use the
Connection
view to define controller-to-device behavior.
  • Select a requested packet interval.
  • Choose a unicast or multicast connection over EtherNet/IP
  • Choose a scheduled or unscheduled connection over ControlNet.
  • Choose to inhibit the device.
  • Configure the controller so that a loss of connection to this device causes a major fault in the controller.
  • View connection faults.
    TIP:
    The data in the
    Connection
    view comes directly from the controller and displays information about the condition of the connection between the controller and the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal