Input view parameters
The
Input
view includes these parameters:
Parameter | Description |
|---|---|
Input | Displays the Input number to which this configuration
applies. |
Input Filter Time Off → On | Defines how long an Off to On input transition must remain in the
On state before the device considers the transition valid. |
Input Filter Time On → Off | Defines how long an On to Off input transition must remain in the
Off state before the device considers the transition valid. |
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback