Device Definition – Windows view parameters

The
Windows
view in the Device Definition dialog includes these parameters:
Parameter
Description
Window
Displays the window number to which this configuration applies.
Mode
Select the counter or SSI variable for the window to operate on.
When Encoder Type is configured as HSC:
  • Count
  • Scaled Count
  • Frequency
  • Scaled Frequency
  • Average Frequency
  • Scaled Average Frequency
  • Pulse Width
  • Average Pulse Width
  • Acceleration
  • Average Acceleration
  • Scaled Acceleration
  • Scaled Average Acceleration
When Encoder Type is configured as SSI:
  • Data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal