View diagnostics information for a port
Use the
Port X diagnostics
dialog box to view diagnostic information
for a port.To view diagnostics information for a port
- On the tab for the device, selectPort Configuration.
- In thePort Configurationview, in thePort Diagnosticscolumn for the port, select
. - InPort X diagnostics, view the diagnostics information as needed.
Provide Feedback