Network view parameters (bridge devices - Duplex)
Use the
Network
view to view information about the Device Level Ring (DLR) network or
the Parallel Redundancy Protocol (PRP) network.The parameters are only available when the application is online, and there is no
communication error in the device profile. Parameters that appear depend on whether the device
profile is online to a DLR device or a PRP device.
WARNING:
PRP/DLR or IP Address switch positions do not match the physical device setting.
This warning appears when the:
- DLR or PRP mode switch changes during runtime
- IP rotary switches change during runtime
Device Level Ring settings
Parameter | Description |
|---|---|
Network Mode | Shows that the device profile is online to a Device Level Ring (DLR) device. |
Network Topology | Displays the current network topology as either:
|
Network Status | Displays the current network status as:
|
Supervisor Status | Displays the status of the supervisor. Only available when Supervisor Mode
is enabled. Available values:
|
Active Ring Supervisor | Displays the IP Address or MAC Address of the Active Ring Supervisor. Only available when the device is in a Ring network. |
Active Supervisor Precedence | Displays the precedence currently assigned to the active ring supervisor. Only available when the device is in a Ring network. |
Ring Faults Detected | Displays the number of ring faults detected on the network since the last power
cycle or counter reset. Only available when the device is a ring supervisor. |
Last Active Node on Port 1 | Displays the IP address or MAC ID of the last node the active ring supervisor can
communicate with on Port 1 when a ring fault has occurred. Only available when the device is a ring supervisor. |
Last Active Node on Port 2 | Displays the IP address or MAC ID of the last node the active ring supervisor can
communicate with on Port 2 when a ring fault has occurred. Only available when the device is a ring supervisor. |
Ring Fault Status | Displays the current condition of the ring fault as either:
Only available when the device is a ring supervisor. |
Enable Supervisor Mode | Indicates that the device is configured as a supervisor on the network. If cleared,
the Supervisor Mode is disabled, and the device is not a supervisor on the
network. |
Reset Ring Faults | Used to reset the device's ring fault count to zero. Only available when the device is a ring supervisor. |
Verify Fault Location | Causes the device to verify the last node fault location on port 1 and port 2 and
update the Last Active Node parameters.The Last Active Node parameters show information from the last fault until
verification of the fault location.Only available when the device is a ring supervisor. |
Clear Rapid Fault | Causes the device to clear the Rapid Faults/Restore Cycles fault. Only available when the device is a ring supervisor and the ring fault condition is
Rapid Fault/Restore Cycles . |
Refresh | Retrieves and displays the latest information from the device. |
Advanced Configuration | Opens Advanced Network Configuration to configure advanced network
properties. |
Parallel Redundancy Protocol settings
The Parallel Redundancy Protocol requires two separate physical networks to operate. These
networks are labeled LAN A and LAN B.
Parameter | Description |
|---|---|
Network Mode | Shows that the device profile is online to a Parallel Redundancy Protocol (PRP)
device. |
Last PRP Fault Timestamp - Port A | Displays the timestamp of the last fault for port A. None displays when
there is no fault for the port.Tip: To ensure the correct timestamp appears, enable the Precision Time Protocol
and synchronize the adapter. |
Last PRP Fault Timestamp - Port B | Displays the timestamp of the last fault for port B. None displays when
there is no fault for the port.Tip: To ensure the correct timestamp appears, enable the Precision Time Protocol
and synchronize the adapter. |
Diagnostics for other PRP nodes | Displays the list of PRP devices detected by the device and the LAN(s) they were
detected on. |
Address | Displays the node's IP Address or MAC Address. |
Node Type | Specifies the node's operating mode.
|
Port A | Displays the status of the node on LAN A.
|
Port B | Displays the status of node on LAN B.
|
Diagnostics | Displays counters and status information for each LAN. |
Network Status | Displays the state of the LAN.
|
Network Fault Count | Displays the number of times the Network Status parameter has changed from
OK to Fault since the last Reset Counters operation or powerup. |
Transmit Count | Displays the number of PRP-tagged frames transmitted over each LAN since the last
Reset Counters operation or powerup. |
Receive Count | Displays the number of PRP-tagged frames received on each LAN since the last Reset
Counters operation or powerup. |
Wrong LAN Count | Displays the number of PRP-tagged frames received on the wrong LAN since the last
Reset Counters operation or powerup. For example, a LAN A PRP-tagged frame is
received on LAN B (or vice versa). Usually indicative of a wire cross-connected from LAN A to LAN B. |
Unique Entry Count | Displays the number of PRP-tagged frames received on one LAN, but not received on
the other LAN, since the last Reset Counters operation or powerup. Usually indicative of a loss of connection or loss of frames on the other LAN. |
Duplicate Entry Count | Displays the number of PRP-tagged frames received on this LAN that were already
received on another LAN since the last Reset Counters operation or powerup. Tip: This count increments during normal operation, and is not an indication of a
fault. |
Multiple Entry Count | Displays the number of PRP-tagged frames for which multiple duplicates were
received on each LAN since the last Reset Counters operation or powerup. Usually indicative of a miss configured network (such as a routing loop). |
Refresh | Retrieves and displays the latest information from the device. |
Reset Counters | Sets the PRP counter values to zero and then refreshes the values displayed on the
tab with the current counter values. |
Provide Feedback