Network view (bridge devices)
Use the
Network
view to view network information. The information shown depends on
whether the device profile is online to a Device Level Ring (DLR) capable device or a Parallel
Redundancy Protocol (PRP) capable device.If the device profile is online to a DLR capable device, use these settings to:
- View whether the network is operating in Linear/Star or Ring network.
- View the current status of the network.
- Enable the device to be a supervisor on the network.
- View the address of the active ring supervisor and the active supervisor precedence.
- View information about the ring faults such as the number of ring faults and the status of the ring faults.
- Reset the ring fault count to zero.
If the device profile is online to a PRP capable device, use these settings to:
- Monitor the health status of each LAN on the PRP network and its attached devices.
- Reset the diagnostic counter.
This information is only available when online, and there is no communication error in the
device profile.
TIP:
For controller devices that have one or more configurable EtherNet port pairs, for example
CompactLogix
5380, Network
is blank except for
Refresh
when the EtherNet/IP Mode setting does not support DLR.Provide Feedback