Disable IP settings set by switches on the device
When using the switches on the device to set the IP address,
IP settings set by switches
on the device
is set automatically.To disable IP settings set by switches on the device
- Change the switch settings on the device.
- Reset the device by either of these two ways:
- Cycling power to the device.
- SelectingReset Devicein theDevice Informationview.
Provide Feedback