Change the bridge device type and revision
Use the
Change type
dialog box to change the bridge device type or
revision (for example, changing from a 1756-EN2T/A EtherNet Bridge device to a 1756-ENBT/A
EtherNet Bridge device).
TIP:
The parameters are unavailable when the profile has pending edits, or when the device is online with the controller in Run mode.
- On the tab for the device, selectOverview.
- In theOverviewview, selectDevice definition.
- InDevice definition, selectChange type.
- InChange type, specify the device type and revision as needed.TIP:Changing the device type will change, delete, or invalidate the device properties that are not valid for the new device type.
- SelectOKto finalize the changes and exit the dialog box.
Provide Feedback