Configure individual input point properties
Configure the properties of the individual input point to eliminate high frequency
oscillations or spikes from input signals for that point.
To configure individual input point properties
- On the tab for the device, expandPoints, and then select an individual point.
- In thePtxxview, fill in the parameters and selectOK.
Provide Feedback