Configure individual output channel properties
Configure the individual output channel so that it can properly connect to Current or Voltage
output types and to multiple output signal ranges.
To configure individual output channel properties
- On the tab for the device, expandChannels, and then select an individual channel.
- In theCh0xview, fill in the parameters and selectOK.
Provide Feedback