Configure alarm properties
Configure alarm properties to alert you when the device exceeds configured high or low
limits.
To configure alarm properties
- On the tab for the device, expandChannels, and then expand an individual channel.
- SelectAlarms.
- In theAlarmsview, fill in the parameters and selectOK.
Provide Feedback