Using the NIST Cybersecurity Framework (CSF) as a risk-based cybersecurity approach is a way to protect against threats effectively and proactively. This approach gives manufacturers a way to develop cybersecurity risk profiles that represent where they are and then create a map forward to the desired end state for their cybersecurity programs.
Register for part one in our seven-part series to learn:
- How to determine your risk profile
- Ways to implement effective risk controls
- Strategies for balancing the residual risk
PLUS – attendees are also given exclusive access to a tool that will quickly identify how you measure up to each area of the NIST CSF.
Additional webinars will be provided to discuss each area of the NIST CSF along with actionable steps to improvement in areas where assessment scores were low.
Don't miss the chance to post your questions to our experts in the live Q&A session at the end of our event.