Architecture

The following examples of SIL 3 and SIL 2 systems show these features:
  • The overall safety function
  • The
    GuardLogix®
    portion of the overall safety function
  • How other devices that operate outside the safety function, such as HMI, are connected
Example SIL 3 System
Example SIL 3 System
Example SIL 2 System
Example SIL 2 System
Example SIL 2 System
Example SIL 2 System
5034-AENTR and 5034-AENTRXT Wiring Diagram
5034-AENTR and 5034-AENTRXT Wiring Diagram
Object Hierarchy
Object Hierarchy
Commission a Safety System
Commission a Safety System
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal