Overhead Lift by Crane or Hoist
All lifting equipment and components (hooks, bolts, lifts, slings, chains, and so forth) must be properly sized and rated to lift and hold the weight of the equipment safely. Follow local codes and guidelines and your company safety procedures when you handle PowerFlex products. Shipment weights can be found on the packing slip that is included with each shipment. See Approximate Weights for PowerFlex 755T Drive Products for approximate weights. Structural angles with lifting holes are affixed to the top of the product enclosures.
ATTENTION:
Risk of injury or equipment damage exists.
- Inspect all lifting hardware for proper attachment before lifting the equipment.
- Do not allow any part of the equipment or lifting mechanism to contact electrically charged conductors or components.
- Do not subject the equipment to high rates of acceleration or deceleration while transporting to the installation site or when lifting.
- Do not allow personnel or their limbs directly underneath the equipment when it is being lifted and mounted.
Provide Feedback