Configuration Tools

Any of the following configuration tools can be used:
  • PowerFlex®
    20-HIM-A6 or 20-HIM-C6S HIM. See the PowerFlex 20-HIM-A6 or 20-HIM-C6S HIM (Human Interface Module) User Manual, publication 20HIM-UM001.
  • Connected Components Workbench
    (CCW) software R10.00 or later.
    Connected Components Workbench
    software is the recommended standalone software tool for use with
    PowerFlex®
    drives. You can obtain a free copy by Internet download at the Product Compatibility and Download Center .
  • Controller configuration software, such as
    RSLogix 5000®
    software, version 20.00 or later, or
    Studio 5000 Logix Designer®
    application, version 21.00 and later.
  • Automatic Device Configuration (ADC), an
    RSLogix 5000®
    software feature, which supports the automatic download of configuration data. The download occurs after the Logix controller establishes an
    EtherNet/IP
    network connection to a
    PowerFlex®
    755TL, 755TR, or 755TM product and its associated peripherals.
  • A computer connection to the
    EtherNet/IP
    network.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal