Configure Safety Enable Circuitry

The drive ships with the safety enable jumper (SAFETY) installed. This jumper must be removed when using the safe torque off or speed monitoring safety options.
NOTE:
Failure to remove the jumper when using either safety option causes the drive to fault when a start command is issued.
An image detailing a jumper location.
IMPORTANT:
Change main control circuit board configurations only when the control pod is de-energized.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal